3. BLE Development Environment and First Application
3.1. Development Environment
3.1.1. Overview
This section first provides an overview for the DA1453x/DA1458x development environment that consists of the:
Arm Keil uVision IDE/Debugger, Arm C/C++ Compiler, and its essential middleware components Keil IDE and the Keil build tools
Arm Segger JTAG cables and software that is fully supported by the Keil environment
DA1453x/DA1458x Software Development Kit (SDK)
The development environment is also supported by a number of other utilities and tools such as:
SmartSnippets™ Toolbox, which is a framework of PC-based utilities to control the DA1453x/DA1458x development kit, and consists of:
Booter that is used to download hex files to DA1453x/DA1458x RAM over UART and to reset the chip to execute from there
Board Setup is used to manage communication with the chip
UART Terminal is available only for connection over UART. After the selected file is successfully downloaded to the DA1453x/DA1458x chip, the ‘Start Terminal’ button is activated and the user can click the button to receive data from UART
Terminal Scripting tool is a Terminal Emulation tool bundled with SmartSnippents Toolbox that enables users to download a firmware and interact with a target device in real time
Power Profiler is used for plotting the current (and associated charge) drawn by the DA1453x/DA1458x on the DK in real time over USB
Battery Lifetime Estimator tool is available for DA1458x families. This tool is used to estimate the battery lifetime for a selected device family
OTP Programmer tool is used to burn the OTP Memory and OTP Header
SPI Flash/EEPROM Programmer is used to download an image file to the SPI Flash Memory or EEPROM
RF Master is an implementation of Bluetooth SIG standardized receiver and transmitter HCI commands and additional custom test HCI commands. RF Master has replaced the Connection Manager tool. RF Master supports the following tests:
LE Tx/Rx
Unmodulated Tx/Rx
Continuous Tx
XTAL
Sleep
The “User Guide” html for all these utilities is available under the “help” drop down menu of the SmartSnippets™ Toolbox application. This is installed by SmartSnippets™ Studio.
3.1.2. Software Development Kit (SDK) Structure
The SDK structure is defined in the following sections.
3.1.2.1. root Directory
The SDK contains the following main directories.
Figure 17 root Directory Structure
3.1.2.2. binaries Directory
This directory holds the executable binaries of the PC applications stored in the host_apps directory as well as the binary file of the production test tool firmware. These binaries are provided so that the developer can run/test the applications with no need to compile the projects.
Figure 18 binaries Directory Structure
3.1.2.3. config Directory
This directory contains the DA1453x/DA1458x configuration files for the SmartSnippets tool and binary/hex files of flash programmer and secondary_boatloader.
3.1.2.4. doc Directory
This directory contains the SDK license files and chm files with the API documentation for each device family.
3.1.2.5. projects Directory
This directory contains the various SDK example projects. The projects directory is divided into two main directories:
host_apps
target_apps
Figure 19 projects Directory Structure
3.1.2.5.1. host_apps Directory
This directory holds example applications that run on an external processor (PC or other CPU). Actually, it contains the proximity and SUOTA initiator applications that run on PCs.
Figure 20 host_apps Directory Structure
3.1.2.5.2. target_apps Directory
This directory holds example applications that run on the DA1453x/DA1458x SoC. Each project directory contains Keil project files, along with the specific project’s source code and configuration files as shown in Figure 21.
Figure 21 target_apps Directory Structure
The ble_examples directory contains DA1453x/DA1458x SoC BLE application examples for “Integrated processor” or “External processor” configuration.
The ble_examples demonstrate the BLE functionality of the DA1453x/DA1458x SoC. The following list describes briefly each BLE example.
ble_app_barebone: BLE example that demonstrates basic BLE procedures such as advertising, connection, connection parameters update and implementation of the device information service. It is based on the “Integrated processor” configuration.
ble_app_profile: BLE example that demonstrates the same as the ble_app_barebone project, plus the implementation of a custom service (128-bit UUID) defined by the user. The application demonstrates only the custom database creation. It is based on the “Integrated processor” configuration.
ble_app_peripheral: BLE example that demonstrates the same as the ble_app_profile. The application also adds some basic interaction over the provided custom service (read/write/notify values). It is based on the “Integrated processor” configuration.
ble_app_sleepmode: BLE example that demonstrates the same as the ble_app_profile. The application adds the use of the sleep mode API, and makes use of the two available sleep modes – Extended sleep mode (with or without OTP copy) with OTP copy. It is based on the “Integrated processor” configuration.
ble_app_security: BLE example that demonstrates the same as the ble_app_profile. The application adds the various security/privacy features. It is based on the “Integrated processor” configuration.
ble_app_ota: BLE example that demonstrates the same as the ble_app_profile. The application adds the over-the-air programming feature. It is based on the “Integrated processor” configuration.
ble_app_all_in_one: only for DA1458x targets, BLE example that combines in one example the features of the previous ble_app_<example> projects. It is based on the “Integrated processor” configuration.
prox_monitor_ext: BLE example that demonstrates the proximity monitor service. It also includes the device information client service. It uses the “External processor” configuration.
prox_reporter: BLE example that demonstrates the proximity reporter service. It also includes the device information server service, the battery server service and the software patching over the air receiver (SUOTAR) service. It uses the “Integrated processor” configuration.
The hci directory contains a DA1453x/DA1458x SoC application example for HCI interface over UART.
hci: example that demonstrates HCI over serial interface that allows the development of the host on a separate processor.
The misc directory contains miscellaneous application examples for the DA1453x/DA1458x SoC. The following list describes briefly each example.
aes: AES Encryption demo application is a simple application example, which demonstrates how the CryptoAPI can be used to encrypt or decrypt user data using the AES algorithm.
ancs_client: only for DA1458x targets, ANCS Client example application is a sample implementation of an Apple Notification Center Service (ANCS) Client.
ble_app_noncon: BLE example that demonstrates non-connectable advertising.
ble_app_lecb: BLE example that demonstrates LE credit based channels.
The peripheral_examples directory contains DA1453x/DA1458x SoC peripheral examples. The examples demonstrate some of the non-BLE functionality of the
DA1453x/DA1458x SoC. The following list describes briefly each peripheral example.
adc: analog to digital conversion example
blinky: blinks a led
i2c: i2c interface example
quadrature_decoder: quadrature decoder example
shared: shared library for peripheral examples
spi: spi interface example
systick: SysTick timer control example
timer0: timer0 control example
timer2: timer2 control example
uart: uart communication example
The Keil projects contained in the ble_examples SDK directories are based on the structure shown in Figure 22.
Figure 22 Project Directory Example Layout
The Keil_5 directory contains the Keil project files *.uvprojx and *.uvoptx.
The src directory contains the user’s application source code and header files (e.g. user_<example_name>.c, user_<example_name>.h or more) and two directories:
config and platform. These two directories contain files that must be included in a user project structure. The names of these
files must not be altered by the user.
Note
The custom_profile directory can be omitted when the user does not use a Custom profile in his application.
Figure 23 src Project Directory Example Layout
da1458x_config_advanced.h: holds DA1453x/DA1458x advanced configuration settings.da1458x_config_basic.h: holds DA1453x/DA1458x basic configuration settings.user_callback_config.h: callback functions that handle various events or operations.user_config.h: holds advertising parameters, connection parameters, etc.user_config_sw_ver.h: holds user-specific information about the software version.user_custs1_def.c: defines the structure of the Custom 1 profile database structure.user_custs_config.c: defines the cust_prf_funcs[] array, which contains the Custom profiles API functions calls.user_modules_config.h: defines which application modules are included or excluded from the user’s application.user_periph_setup.h: holds hardware-related settings.user_profiles_config.h: defines which BLE profiles (Bluetooth SIG adopted or custom ones) will be included in the user’s application.user_periph_setup.c: source code file that handles peripheral configuration and initialization.
3.1.2.6. sdk Directory
This directory holds the core files of the SDK. The directory structure of the core SDK modules is depicted below.
Figure 24 sdk Directory Structure
3.1.2.6.1. app_modules Directory
This directory holds the application source and header files.
api: contains the application header files.src: contains the application’s project specific code for some BLE profiles and handling functions for BLE operations, like advertising, connection, security/encryption, etc.
Important
New Features Starting from SDK version 6.0.24
1/ Added application files for profiles
Blood Pressure Profile (BLP)
Health Thermometer Profile (HTP)
Time Profile (TIP)
Heart Rate Profile (HRP)
Running Speed and Cadence Profile (RSCP)
HID Over Gatt Profile Device (HOGPD)
Phone Alert Status Profile (PASP)
Location and Navigation Profile (LANP)
Cycling Speed and Cadence Profile (CSCP)
Scan Parameters Profile (SCPP)
Alert Notification Profile (ANP)
2/ Secure storage features: we introduced two app modules: app_easy_storage.c and app_easy_crypto.c
Encryption module: provides an easy-to-use API for encryption functions.
Storage module: provides an easy-to-use API for memory storage functions.
3.1.2.6.2. ble_stack Directory
This directory contains BLE stack related files.
3.1.2.6.3. common_project_files Directory
This directory contains the following folders plus three configuration header files.
Figure 25 common_project_files Directory Structure
ldscripts: contains GNU LD linker scripts for the DA1453x/DA1458x SoC.misc: contains the ROM symbol definition files. This file will be used as input into the linker to create the final executable. The executable files, as well as the compilation outputs, are saved in a newly created directory named out_DA14531, out_DA14531_01,out_DA14535, out_DA14585 or out_DA14586, depending on the selected SoC.scatterfiles: contains Keil scatter files for the DA1453x/DA1458x SoC.
The three configuration files are:
da1458x_periph_setup.h: definitions of the used hardware platform.da1458x_scatter_config.h: definitions of the memory layout.da1458x_stack_config.h: definitions of the stack.
3.1.2.6.4. platform Directory
This directory contains the platform specific files for the Arm Cortex-M0 processor and its supported peripherals (BLE, serial interfaces, GPIOs, etc.).
arch: contains the system files and the main() application function.core_modules: contains core system modules, like the kernel that implements the message handling, the GTL implementation, the non-volatile data storage manipulation, RF drivers, etc.driver: contains all the supported drivers for the Arm Cortex-M0 peripherals.include: header files of the core source files.system_library: contains the object files of the patched ROM functions and the code for the RF calibration. More information for the patched functions is given in the Release Notes of the SDK distribution.utilities: contains the system utilities modules, like OTP header and OTP Configuration Script, it contains also the Flexible Software Package (FSP) external processor user applicatioon source code.
3.1.2.7. third_party Directory
This directory holds any third-party source file that is used within the SDK.
Figure 26 third_party Directory Structure
3.1.2.8. utilities Directory
This directory holds utilities and tools that supplement the SDK.
Figure 27 utilities Directory Structure
flash_programmer: Flash programmer for DA1453x/DA1458x SoC. For more detailed information, see Appendix Section 6.4.prod_test: production test utility. For more detailed information, see Appendix Section 6.3.secondary_bootloader: secondary bootlader utility. For more detailed information, see Appendix Section 6.2.mkimage: make image tool. For more detailed information, see Appendix Section 6.2.7.4.
3.2. Proximity Reporter: Your First Bluetooth Low Energy Application
3.2.1. Application Description
The Proximity profile defines the behavior of a Bluetooth device when it moves away from a peer device so that either the connection is dropped or the path loss increases above a predefined level. Either of these conditions will cause an immediate alert. This alert can be used to notify the user that the devices have become separated.
The Proximity profile can also be used to define the behavior of two devices which are coming closer together such that either a connection is made or the path loss decreases below a predefined level.
The Proximity profile defines two roles:
Proximity Monitor (PM): The Proximity Monitor shall be a GATT client
Proximity Reporter (PR): The Proximity Reporter shall be a GATT server
This section describes only the Proximity Reporter application.
Note
The Proximity Reporter application supports entering deep sleep mode (e.g. shipping mode – when the device is not yet activated by the end customer). Upon wakeup, application execution will not restart. To restart execution after wakeup the developer must program the code to OTP or to external flash memory resource (e.g. SPI flash).
3.2.2. User Interface
The application will notify the user when an alert indication, link loss and immediate alert are triggered. The Alert Notification will be:
High level alert: A fast (500 ms) LED blinkingLow level alert: A slow (1500 ms) LED blinking
The user can stop alert notification by pressing a push button. The selected
LED and push button (port and pin number of the DA1453x/DA1458x) are defined
by the user configuration depending on the target device (DA1453x/DA1458x).
The user file user_periph_setup.h holds the peripheral configuration settings
of the LED and push button.
3.2.3. Loading the Project
The Proximity Reporter application, in particular, may be built and run, using
any of the following IDEs, out of the box: Keil; e² studio, Eclipse AND IAR.
For each of the aforementioned IDEs, there is a dedicated folder – including all
the necessary project files – residing in
<sdk_root_directory>\projects\target_apps\ble_examples\prox_reporter, namely
Keil_5, Eclipse, e² studio and IAR, respectively.
For the sake of simplicity, we will proceed to refer to the Keil IDE, unless explicitly mentioning e² studio, Eclipse or IAR.
Figure 28 shows the Keil project layout with emphasis on the user related files. These are included in the Keil project folders
user_config, user_platform and user_app. These folders contain the user configuration files of the Proximity Reporter
application.
Figure 28 Proximity Reporter Keil Project Layout
Important
e² studio SDK 6 Getting Started Guide
To start building a fully working solution on e2 studio and SDK6 you can refer to the e² studio SDK 6 Getting Started Guide.
3.2.4. Going Through the Code
3.2.4.1. Basic Operation
The Proximity Reporter application supports the following services:
Immediate Alert service (UUID 0x1802)
Link Loss service (UUID 0x1803)
Tx Power service (UUID 0x1804)
Device Information service (UUID 0x180A)
Battery service (UUID 0x180F)
Software Update Over The Air Receiver (SUOTAR) service (UUID 0xFEF5)
The Proximity Reporter application has the following features:
Two levels of Alert Indications. Low/High -> Slow/Fast green LED blinking.
500 ms advertising interval.
Extended sleep without OTP copy mode after 3 minutes of inactivity.
Push button.
Stop Alert indications.
Exit Extended sleep without OTP copy mode.
Pairing / bonding / encryption.
Supports Extended / Deep sleep mode/ Hibernation / Stateful hibernation (the last two modes being applicable to DA1453x only).
The Proximity Reporter operation is implemented in C source file user_proxr.c.
3.2.4.2. Initialization
The previously mentioned Keil project folders (user_config, user_platform and user_app), contain the files that initialize and configure the Proximity Reporter application.
user_config
da1458x_config_advanced.h: holds DA1453x/DA1458x advanced configuration settingsda1458x_config_basic.h: holds DA1453x/DA1458x basic configuration settingsuser_callback_config.h: callback functions that handle various events or operationsuser_config.h: holds advertising parameters, connection parameters, etc.user_modules_config.h: defines which application modules are included or excluded from the user’s application For example:
#define EXCLUDE_DLG_DISS (0)
In this case the Device information application profile is included in the core SDK and the SDK takes care of the Device information application profile message handling internally.
#define EXCLUDE_DLG_DISS (1)
In this case the Device information application profile is excluded from the core SDK. The user application must take care of the Device information application profile message handling.
user_profiles_config.hdefines which BLE profiles (Bluetooth SIG adopted or custom ones) will be included in the user’s application. The BLE profiles that are included in theuser_profile_config.hfile are:
/***************************************************************************************/
/* Used BLE profiles (used by "rwprf_config.h"). */
/***************************************************************************************/
#define CFG_PRF_DISS
#define CFG_PRF_PXPR
#define CFG_PRF_SUOTAR
#define CFG_PRF_BASS
CFG_PRF_DISS: includes the Device Information service
CFG_PRF_PXPR: includes the Immediate Alert, Link Loss and Tx Power services
CFG_PRF_SUOTAR: includes the Software Update Over The Air service
CFG_PRF_BASS: includes the Battery service
user_platform
user_periph_setup.h: holds hardware related settings relative to the Development Kituser_periph_setup.c: source code file that handles peripheral (GPIO, UART, etc.) configuration and initialization relative to the selected Development Kit
user_app
user_proxr.c & user_proxr.h: proximity reporter application source and header files
These files provide the main application, and define what to do when a button is pressed, when a connection is dropped or when adverting stops. These are all implemented as user callbacks as described in the next section. The trigger mechanism used to wake up from deep sleep or hibernation is also defined, as it is demonstrated in the proximity reporter application:
CFG_DEEP_SLEEP_WAKEUP_GPIO– An external wake up interrupt (instantaneous button press) triggers the system to wake up from deep sleep.CFG_DEEP_SLEEP_WAKEUP_POR– A power on reset (POR) source (continuous button press for approximately 3 seconds, by default) triggers the system to wake up from deep sleep.CFG_DEEP_SLEEP_WAKEUP_RTC– An RTC interrupt triggers the system to wake up from deep sleep after 10 seconds (applicable to DA1453x only).CFG_DEEP_SLEEP_WAKEUP_TIMER1– A Timer1 interrupt triggers the system to wake up from deep sleep after 136.47 ms (= 2047 clock cycles * (1 / 15 ms/clock cycle)) if Timer1 uses the internal RCX oscillator whose typical frequency is 15 kHz or after 62.47 ms (= 2047 clock cycles * (1 / 32.768 ms/clock cycle)) if Timer1 uses an external XTAL oscillator whose typical frequency is 32.768 kHz (applicable to DA1453x only).CFG_APP_GOTO_HIBERNATION– Wake up the system from specific GPIO (P0_3) (applicable to DA1453x only).CFG_APP_GOTO_STATEFUL_HIBERNATION– Wake up the system from specific GPIO (P0_3) (applicable to DA1453x only).
Note
When defining either CFG_APP_GOTO_HIBERNATION or CFG_APP_GOTO_STATEFUL_HIBERNATION,
CFG_SPI_FLASH_ENABLE in da1458x_config_basic.h shall be undefined.
Otherwise, a compilation error –
“Config error: Can not define both CFG_SPI_FLASH_ENABLE and
CFG_APP_GOTO_HIBERNATION/CFG_APP_GOTO_STATEFUL_HIBERNATION.” – will occur.
Furthermore, if SUOTAR is to be used, CFG_I2C_EEPROM_ENABLE in
da1458x_config_basic.h shall be defined instead (if not, a compilation
error – “SUOTA application is enabled but both I2C EEPROM and SPI Flash are
disabled” – will occur). If SUOTAR will not be used,
#define EXCLUDE_DLG_SUOTAR (1) in user_modules_config.h shall be
defined and CFG_PRF_SUOTAR in user_profiles_config.h shall be undefined.
Note
For more information about the Hibernation mode of DA1453x, see the respective datasheet.
Note
If none of the above-mentioned DEEP_SLEEP flags is defined, the system does not enter
the Deep sleep mode, but the selected Extended sleep mode (as defined in the user_config.h file).
The system exits the Extended sleep mode, if the user presses the button that causes advertising to restart.
In the case of DA1453x, the system may alternatively exit the Extended sleep mode
through an RTC interrupt (if CFG_EXT_SLEEP_WAKEUP_RTC is defined) or a
Timer1 interrupt (if CFG_EXT_SLEEP_WAKEUP_TIMER1 is defined).
Note
When the system enters the Deep sleep mode, all the RAM blocks are switched off. No application code or data are retained.
Note
When the system exits the Deep sleep mode, the boot rom code is executed and the application code has to be loaded again, either from OTP memory or external memory source (e.g. SPI flash).
3.2.4.3. Events Processing and Callbacks
Several events can occur during the lifetime of the Bluetooth low energy application and these events need to be handled in a specific manner. The application is responsible to select which events and operations to handle and which to leave to be handled by the default SDK behavior.
The SDK uses a mechanism that registers callbacks for every event or operation
that defines the system behavior. The C header file user_callback_config.h,
which is part of the user application, contains the registration of callback functions.
The Proximity Reporter application registers the following callback functions:
General BLE events:
static const struct app_callbacks user_app_callbacks = {
.app_on_connection = default_app_on_connection,
.app_on_disconnect = user_app_on_disconnect,
.app_on_update_params_rejected = NULL,
.app_on_update_params_complete = NULL,
.app_on_set_dev_config_complete = default_app_on_set_dev_config_complete,
.app_on_adv_nonconn_complete = NULL,
.app_on_adv_undirect_complete = app_advertise_complete,
.app_on_adv_direct_complete = NULL,
.app_on_db_init_complete = default_app_on_db_init_complete,
.app_on_scanning_completed = NULL,
.app_on_adv_report_ind = NULL,
.app_on_get_dev_name = default_app_on_get_dev_name,
.app_on_get_dev_appearance = default_app_on_get_dev_appearance,
.app_on_get_dev_slv_pref_params = default_app_on_get_dev_slv_pref_params,
.app_on_set_dev_info = default_app_on_set_dev_info,
.app_on_data_length_change = NULL,
.app_on_update_params_request = default_app_update_params_request,
.app_on_generate_static_random_addr = default_app_generate_static_random_addr,
.app_on_svc_changed_cfg_ind = NULL,
.app_on_get_peer_features = NULL,
#if (BLE_APP_SEC)
.app_on_pairing_request = default_app_on_pairing_request,
.app_on_tk_exch = default_app_on_tk_exch,
.app_on_irk_exch = NULL,
.app_on_csrk_exch = NULL,
.app_on_ltk_exch = default_app_on_ltk_exch,
.app_on_pairing_succeeded = NULL,
.app_on_encrypt_ind = NULL,
.app_on_encrypt_req_ind = NULL,
.app_on_security_req_ind = NULL,
.app_on_addr_solved_ind = NULL,
.app_on_addr_resolve_failed = NULL,
#if !defined (__DA14531_01__) && !defined (__DA14535__)
.app_on_ral_cmp_evt = NULL,
.app_on_ral_size_ind = NULL,
.app_on_ral_addr_ind = NULL,
#endif // not for DA14531-01, DA14535
};
#endif // (BLE_APP_SEC)
The structure above defines whether each event is processed by a default handler,
by a user-defined handler or is not processed at all (NULL entries). The user
defined handlers (e.g. app_advertise_complete()) are defined in a C source file user_proxr.c.
System specific events:
static const struct arch_main_loop_callbacks user_app_main_loop_callbacks = {
.app_on_init = default_app_on_init,
// By default the watchdog timer is reloaded and resumed when the system wakes up.
// The user has to take into account the watchdog timer handling (keep it running,
// freeze it, reload it, resume it, etc.), when the app_on_ble_powered() is being
// called and may potentially affect the main loop.
.app_on_ble_powered = NULL,
// By default the watchdog timer is reloaded and resumed when the system wakes up.
// The user has to take into account the watchdog timer handling (keep it running,
// freeze it, reload it, resume it, etc), when the app_on_system_powered() is being
// called and may potentially affect the main loop.
.app_on_system_powered = NULL,
.app_before_sleep = NULL,
.app_validate_sleep = NULL,
.app_going_to_sleep = NULL,
.app_resume_from_sleep = NULL,
};
The above structure defines that a certain event is processed by a default handler or by a user-defined handler or is not processed at all (NULL entries). In this case the default SDK application initialization function is used and all other events are not handled.
BLE operations:
static const struct default_app_operations user_default_app_operations = {
.default_operation_adv = default_advertise_operation,
};
The above structure defines that a certain operation is processed by a default handler or by a user-defined handler or is not processed at all (NULL entries). In this case only the default advertising operation is used.
Note
DA1453x/DA1458x SDK supports the URI data type in advertising and/or scan response packets. The URI data type allows the representation of a URI. A Uniform Resource Identifier (URI) is a compact sequence of characters that identifies an abstract or physical resource, as defined in IETF STD66.
An example implementation of a URI can be seen in the advertising data of
the proximity reporter demo application. Please check ADV_TYPE_URI in
the USER_ADVERTISE_DATA definition in the usef_config.h file of
the project.
#define USER_ADVERTISE_DATA ("\x09"\
ADV_TYPE_COMPLETE_LIST_16BIT_SERVICE_IDS\
ADV_UUID_LINK_LOSS_SERVICE\
ADV_UUID_IMMEDIATE_ALERT_SERVICE\
ADV_UUID_TX_POWER_SERVICE\
ADV_UUID_SUOTAR_SERVICE\
"\x10"\
ADV_TYPE_URI\
"\x16\x2F\x2F\x77\x77\x77\x2E\x69\x61\x6E\x61\x2E\x6F\x72\x67")
3.2.5. BLE Application Abstract Code Flow
Figure 29 shows the abstract code
flow diagram of the Proximity Reporter application. The diagram depicts the SDK
interaction with the callback functions registered in user_callback_config.h
and the functions implemented in user_proxr.c. The user configuration block
purely executes the callbacks defined for these operations and events. It
simply calls the default handlers for each of the events until adverting is
started. The first user-defined callback is app_advertise_complete(), which is
plugged into the callback table as .app_on_adv_undirect_complete().
Figure 29 Proximity Reporter - User Application Code Flow
The default advertising function is default_advertise_operation(), as
shown in the following code snippet, and is located
in <sdk_default_directory>\sdk\app_modules\src\app_default_hnd.
void default_advertise_operation(void)
{
if (user_default_hnd_conf.adv_scenario == DEF_ADV_FOREVER)
{
app_easy_gap_undirected_advertise_start();
}
else if (user_default_hnd_conf.adv_scenario == DEF_ADV_WITH_TIMEOUT)
{
app_easy_gap_undirected_advertise_with_timeout_start(user_default_hnd_conf.advertise_period, NULL);
}
}
The parameters of the default_advertise_operation() can be configured in
the user_config.h file located in <sdk_default_directory>\projects\target_apps\ble_examples\prox_reporter\src\config
as shown in the following code snippet. This specifies that the advertising is to last 3 minutes and that there is no security defined for the connection.
static const struct default_handlers_configuration user_default_hnd_conf = {
// Configure the advertise operation used by the default handlers
// Possible values:
// - DEF_ADV_FOREVER
// - DEF_ADV_WITH_TIMEOUT
.adv_scenario = DEF_ADV_WITH_TIMEOUT,
// Configure the advertise period in case of DEF_ADV_WITH_TIMEOUT.
// It is measured in timer units (3 min). Use MS_TO_TIMERUNITS macro to convert
// from milliseconds (ms) to timer units.
.advertise_period = MS_TO_TIMERUNITS(180000),
// Configure the security start operation of the default handlers
// if the security is enabled (CFG_APP_SECURITY)
// Possible values:
// - DEF_SEC_REQ_NEVER
// - DEF_SEC_REQ_ON_CONNECT
.security_request_scenario = DEF_SEC_REQ_NEVER
};
The app_advertise_complete() user function is used to define the specific
behavior that the application has when the 3-minute advertising period is finished.
As shown in the code snippet below, this is to stop any active alert, enable a
button to wake up from deep sleep and then to enter deep sleep. For DA1453x the
wake-up source may alternatively be RTC or Timer1.
It should be highlighted that two power modes have been introduced for DA1453x only, namely hibernation and stateful hibernation. Both modes are clockless ones, while RAM block(s) may or may not be retained:
When in hibernation, no code/data is retained (see the hibernation mode configuration in
user_proxr.h).When in stateful hibernation, all three RAM blocks are retained (see the stateful hibernation mode configuration in
user_proxr.h). As soon as the device wakes up from stateful hibernation, both the processor state and system register content will be restored – code execution will resume from the point the device went to stateful hibernation onwards: the orange LED – D5 on the 376-18-B Motherboard – will be turned on for a couple of seconds. Then, the device will get idle (in theARCH_SLEEP_OFFcase) or go to extended sleep (in theARCH_EXT_SLEEP_ONcase), waiting for an interrupt to occur – by pressing the SW2 button on the 376-18-B Motherboard, the device will get active and restart advertising.
void app_advertise_complete(const uint8_t status)
{
if ((status == GAP_ERR_NO_ERROR) || (status == GAP_ERR_CANCELED))
{
#if (BLE_PROX_REPORTER)
app_proxr_alert_stop();
#endif
}
if (status == GAP_ERR_CANCELED)
{
arch_ble_ext_wakeup_on();
#if defined (__DA14531__)
// Configure PD_TIM
#if defined (CFG_EXT_SLEEP_WAKEUP_RTC) || defined (CFG_EXT_SLEEP_WAKEUP_TIMER1) || \
defined (CFG_DEEP_SLEEP_WAKEUP_RTC) || defined (CFG_DEEP_SLEEP_WAKEUP_TIMER1)
// Ensure PD_TIM is open
SetBits16(PMU_CTRL_REG, TIM_SLEEP, 0);
// Wait until PD_TIM is opened
while ((GetWord16(SYS_STAT_REG) & TIM_IS_UP) != TIM_IS_UP);
#else
// Close PD_TIM
SetBits16(PMU_CTRL_REG, TIM_SLEEP, 1);
// Wait until PD_TIM is closed
while ((GetWord16(SYS_STAT_REG) & TIM_IS_DOWN) != TIM_IS_DOWN);
#endif
#endif
#if defined (CFG_APP_GOTO_DEEP_SLEEP)
// Put system into deep sleep
put_system_into_deep_sleep();
#elif defined (__DA14531__) && defined (CFG_APP_GOTO_HIBERNATION)
// Put system into hibernation
arch_set_hibernation(HIB_WAKE_UP_PIN_MASK,
CFG_HIBERNATION_RAM1,
CFG_HIBERNATION_RAM2,
CFG_HIBERNATION_RAM3,
CFG_HIBERNATION_REMAP,
CFG_HIBERNATION_PAD_LATCH_EN);
#elif defined (__DA14531__) && defined (CFG_APP_GOTO_STATEFUL_HIBERNATION)
// Put system into stateful hibernation
arch_set_stateful_hibernation(HIB_WAKE_UP_PIN_MASK,
CFG_STATEFUL_HIBERNATION_RAM1,
CFG_STATEFUL_HIBERNATION_RAM2,
CFG_STATEFUL_HIBERNATION_RAM3,
CFG_STATEFUL_HIBERNATION_REMAP,
CFG_STATEFUL_HIBERNATION_PAD_LATCH_EN);
#if (DEVELOPMENT_DEBUG)
// Turn on the orange LED (D5 on the 376-18-B Motherboard)
SetWord16(P09_MODE_REG, ((uint32_t) OUTPUT) | ((uint32_t) PID_GPIO));
SetWord16(P0_SET_DATA_REG, 1 << GPIO_ALERT_LED_PIN);
// Keep it on for a couple of seconds
for (uint32_t i = 4*2000000; i != 0; i--)
{
__NOP();
}
// Turn it off
SetWord16(P0_RESET_DATA_REG, 1 << GPIO_ALERT_LED_PIN);
#endif // DEVELOPMENT_DEBUG
// Configure button to trigger wake-up interrupt from extended sleep
app_button_enable();
#elif defined (__DA14531__) && defined (CFG_EXT_SLEEP_WAKEUP_RTC)
// Configure RTC to trigger wake-up interrupt from extended sleep
configure_rtc_wakeup();
#elif defined (__DA14531__) && defined (CFG_EXT_SLEEP_WAKEUP_TIMER1)
// Configure TIMER1 to trigger wake-up interrupt from extended sleep
configure_timer1_wakeup();
#else
// Configure button to trigger wake-up interrupt from extended sleep
app_button_enable();
#endif
}
}
Note
As far as stateful hibernation is concerned, besides defining CFG_APP_GOTO_STATEFUL_HIBERNATION
in user_proxr.h, CFG_STATEFUL_HIBERNATION shall be defined as well in the
project (assembly) settings, as shown in Figure 30,
Figure 32, and
Figure 33 for Keil, Eclipse,
and IAR IDEs, respectively.
Figure 30 Defining CFG_STATEFUL_HIBERNATION in the Keil IDE
Figure 31 Defining CFG_STATEFUL_HIBERNATION in the e² studio IDE
Figure 32 Defining CFG_STATEFUL_HIBERNATION in the Eclipse IDE
Figure 33 Defining CFG_STATEFUL_HIBERNATION in the IAR IDE
3.2.6. Building the Project for Different Targets
The Proximity Reporter application can be built for different target processors, DA14585, DA14586, DA14531, DA14531_01, DA14535 and DA14533.
The selection is done with the Keil tool as shown in Figure 34.
Figure 34 Building the Project for Different Targets
In order to build proximity reporter project for DA14533 target, you select the DA14535 target and then add DA14533 define __DA14533__.
Figure 35 Building the Project for DA14533 Target
After the proper selection of the target processor, the application is ready to be built.
The Proximity Reporter application does not use the UART and so the only jumpers that must be present are those for the debugger interface as mentioned in Table 5.
Target |
SW_CLK PIN |
SW_CLK PIN DK connection |
SW_DIO PIN |
SD_DIO PIN DK connection |
|---|---|---|---|---|
DA1458x |
SW_CLK |
Connect J1.21 with J1.22 |
SW_DIO |
Connect J1.23 with J1.24 |
DA1453x |
P0_2 |
Connect J1.21 with J1.22 |
P0_10 |
Connect J1.23 with J1.24 |
3.2.7. Interacting with BLE Application
The SmartBond™ application, available on iOS or Android, is a mobile application that works as a generic tool for interacting with Bluetooth® Low Energy devices. It used to scan for, and connect to, the DIALOG-PRXR. The iPhone/Android mobile acts as a BLE Central and the application as a BLE Peripheral.
Figure 36 Smartbond Application Connected to Proximity Reporter Application